:LTESt:MEASure:SWAVeform:FUNCtion{N}:STATe

Command Syntax

:LTESt:MEASure:SWAVeform:FUNCtion{1:64}:STATe {DISK | MEMory | OFF}

Query Syntax

:LTESt:MEASure:SWAVeform:FUNCtion{1:64}:STATe?

Query Response

{DISK | MEM | OFF}

Description

Saves a function waveform to a file or memory location after the measurement limit test acquires the specified number of failures. The following command arguments are available:

DISK
Saves the waveform to a file. Use the :LTESt:MEASure:SWAVeform:FUNCtion{N}:FNAMe command to specify the file name.
MEMory
Saves the waveform to a memory location. Use the :LTESt:MEASure:SWAVeform:FUNCtion{N}:WMEMory command to specify the memory location.
OFF
Turns off the saving of a common-mode waveform.