:LTESt:MEASure:SWAVeform:FUNCtion{N}:WMEMory
Command Syntax
:LTESt:MEASure:SWAVeform:FUNCtion{1:64}:WMEMory WMEMory{1:8}
Query Syntax
:LTESt:MEASure:SWAVeform:FUNCtion{1:64}:WMEMory?
Description
Upon completion of an measurement limit test, selects a waveform memory as a destination to save a function waveform. Use the :LTESt:MEASure:SWAVeform:DIFF{N}:STATe command to enable and disable waveform reporting for the channel. Use the :LTESt:MEASure:MLIMit:STATe command to turn off the measurement limit test.