:LTESt:MEASure:SWAVeform:CMODe{N}:WMEMory

Command Syntax

:LTESt:MEASure:SWAVeform:CMODeN:WMEMory WMEMory{1:8}

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:LTESt:MEASure:SWAVeform:CMODeN:WMEMory?

Description

Upon completion of an measurement limit test, selects a waveform memory as a destination to save a common-mode waveform. Use the :LTESt:MEASure:SWAVeform:CMODe{N}:STATe command to enable and disable waveform reporting for the channel. Use the :LTESt:MEASure:MLIMit:STATe command to turn off the measurement limit test