:LTESt:MTESt:SWAVeform:DIFF{N}:STATe
Command Syntax
:LTESt:MTESt:SWAVeform:DIFF{N}:STATe {DISK | MEMory | OFF}
{N} identifies the differential waveform, which must be selected from "<connection1-8>_<ch1,3,5,7>". For example, the differential waveform of connection 4 channels 1 and 2 would be identified as DIFF4_1.
Query Syntax
:LTESt:MTESt:SWAVeform:DIFF{N}:STATe?
Query Response
{DISK | MEM | OFF}
Description
Saves a differential waveform to a file after the mask limit test acquires the specified number of failures. Use the :LTESt:MTESt:SWAVeform:DIFF{N}:FNAMe command to specify the file name.