:LTESt:MTESt:SWAVeform:DIFF{N}:FNAMe
Command Syntax
:LTESt:MTESt:SWAVeform:DIFFN:FNAMe "<path substitution string>\subfolder\filename"
Where:
- DIFFN identifies the channel as in DIFF1_1, DIFF1_3, …, DIFF8_7.
- "<path substitution string> is a string that expands into a specific file path. For example, %USER_DATA_DIR%.
- "subfolder" is an optional path folder. For example, %USER_DATA_DIR%\Waveforms.
- "filename" is a string without the filename extension.
Query Syntax
:LTESt:MTESt:SWAVeform:DIFFN:FNAMe?
Description
Specifies the file name (including path but excluding a filename extension) for saving a differential waveform file for an acquisition limit test. To specify the file type use the :LTESt:MTESt:SWAVeform:DIFF:FTYPe command. This results in the correct filename extension being appended to the filename. This command supports the DEFault common child command.
If a correct filename extension is included in the filename that is sent with the :LTESt:ACQuire:SWAVeform:DIFF:FNAMe command, the extension is ignored and will not be included in the filename. If an incorrect filename extension is included in the filename, a SCPI error will occur similar to this example:
17,"Instrument Error;"".txt"" is not a valid extension for Waveform File. Using extension "".csv""."
Therefore, avoid including an extension when specifying the filename. If you want to check the validity of the filetype, check for a SCPI error after sending the :LTESt:MTESt:SWAVeform:DIFF:FTYPe command.
Use the :LTESt:MTESt:SWAVeform:DIFF{N}:STATe command to enable and disable waveform reporting for the channel. To enable or disable acquisition limit tests, use the :LTESt:LLINe:TEST{N}:STATe command.
Default User Folder
The default folder for storing differential waveform files is in %USER_DATA_DIR%\Waveforms as shown in this picture. It is good practice to include a path substitution string with the filename. For example, %USER_DATA_DIR%\Waveforms\filename.
File names must include a path when using the child :FNAMe command. The :FNAMe command is not affected by a Default Setup or Factory Default.
Specifying a path using a path substitution string in the filename ensures that the file will be saved in (or loaded from) the standard user-data folder. Failure to use a path substitution string may result either in a file created in an parent folder or a file error.