:LTESt:MTESt:SWAVeform:FUNCtion{N}:STATe

Command Syntax

:LTESt:MTESt:SWAVeform:FUNCtion{1:64}:STATe {DISK | MEMory | OFF}

Query Syntax

:LTESt:MTESt:SWAVeform:FUNCtion{1:64}:STATe?

Query Response

{DISK | MEM | OFF}

Description

Saves a function waveform to a file after the mask limit test acquires the specified number of failures. Use the :LTESt:MTESt:SWAVeform:FUNCtion{N}:FNAMe command to specify the file name.