:LTESt:MTESt:SWAVeform:DIFF{N}:WMEMory
Command Syntax
:LTESt:MTESt:SWAVeform:DIFF{N}:WMEMory WMEMory{1:8}
{N} identifies the differential waveform, which must be selected from "<connection1-8>_<ch1,3,5,7>". For example, the differential waveform of connection 4 channels 1 and 2 would be identified as DIFF4_1.
Query Syntax
:LTESt:MTESt:SWAVeform:DIFF{N}:WMEMory?
Description
Upon completion of an mask limit test, selects a waveform memory as a destination to save a differential waveform. Use the :LTESt:MTESt:SWAVeform:DIFF{N}:STATe command to enable and disable waveform reporting for the channel.