:LTESt:MTESt:SWAVeform:CHANnel{N}:WMEMory
Command Syntax
:LTESt:MTESt:SWAVeform:CHANnel{N}:WMEMory WMEMory{1:8}
CHANnel{N} identifies the channel as in CHANnel1_1, CHANnel1_2, …, CHANnel8_8.
Query Syntax
:LTESt:MTESt:SWAVeform:CHANnel{N}:WMEMory?
Description
Upon completion of an mask limit test, selects a waveform memory as a destination to save a channel waveform. Use the :LTESt:MTESt:SWAVeform:CHANnel{N}:STATe command to enable and disable waveform reporting for the channel.