:LTESt:MTESt:SWAVeform:CHANnel{N}:STATe
Command Syntax
:LTESt:MTESt:SWAVeform:CHANnel{N}:STATe {DISK | MEMory | OFF}
CHANnel{N} identifies the channel as in CHANnel1_1, CHANnel1_2, …, CHANnel8_8.
Query Syntax
:LTESt:MTESt:SWAVeform:CHANnel{N}:STATe?
Query Response
{DISK | MEM | OFF}
Description
Saves a channel waveform to a file after the mask limit test acquires the specified number of failures. Use the :LTESt:MTESt:SWAVeform:CHANnel{N}:FNAMe command to specify the file name.