:MEASure:EYE:PAM:PPAMplitude:STATus?
Query Syntax
:MEASure:EYE:PAM:PPAMplitude:STATus?
Query Response
{CORR | INV | QUES}
CORR- The measurement result is correct.
INV- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
QUES- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the :MEASure:EYE:PAM:PPAMplitude measurement. Use the :MEASure:EYE:PAM:PPAMplitude:STATus:REASon? child query to determine the reason for a invalid or questionable measurement.