:MEASure:EYE:PAM:PPAMplitude:THRatio
Command Syntax
:MEASure:EYE:PAM:PPAMplitude:THRatio <ratio>
Query Syntax
:MEASure:EYE:PAM:PPAMplitude:THRatio?
Description
Enters the hit ratio used by the Pk-Pk Amplitude measurements. The default hit ratio is 1e-2 which is called out in the IEEE 802.3cu standard.