:MEASure:EYE:PAM:PPAMplitude:UNITs

Command Syntax

:MEASure:EYE:PAM:PPAMplitude:UNITs {WATT | DBM | VOLT}

Query Syntax

:MEASure:EYE:PAM:PPAMplitude:UNITs?

Description

Sets the amplitude units for the Pk-Pk Amplitude measurement (:MEASure:EYE:PAM:PPAMplitude). Units can be Watts (WATT) or dBM (DBM) for an optical signal and Volts (VOLT) for an electrical signal.