:MEASure:EYE:PAM:PPAMplitude:SOURce
Command Syntax
:MEASure:EYE:PAM:PPAMplitude:SOURce <rte_source>
Where <rte_source> can be one of the following:
ECHannel{N}— Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>" from which the real-time eye was created. With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 isECHannel4_2.EDIFf{N}— Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>" from which the real-time eye was created. With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) isEDIFf5_3.ECMode{N}— Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>" from which the real-time eye was created. With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) isECMode5_3.EFUNction{1:64}EWMemory{1:8}CGMemory{1:8}— If the Color-Grade/Gray Scale memory contains a real-time eye.
Query Syntax
:MEASure:EYE:PAM:PPAMplitude:SOURce?
Query Response
<rte_source>
Description
Selects the source waveform on which to perform the :MEASure:EYE:PAM:PPAMplitude measurement.