:MEASure:EYE:PAM:PPAMplitude:STATus:DETails?
Query Syntax
:MEASure:EYE:PAM:PPAMplitude:STATus:DETails?
Description
Returns a string that may provide additional details for a failed :MEASure:EYE:PAM:PPAMplitude measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :MEASure:EYE:PAM:PPAMplitude:STATus:REASon?. Use the :MEASure:EYE:PAM:PPAMplitude:STATus? parent query to determine if the measurement has failed.