:MEASure:JITTer:JITTer:UNITs
Command Syntax
:MEASure:JITTerN:JITTer:UNITs {SECond | UINTerval}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:JITTer:UNITs?
Description
Sets the units of measure for the jitter measurements to either Second (s) or Unit Interval (UI).