:MEASure:PJITter:HISTogram:COMPosite
Command Syntax
:MEASure:PJITterN:HISTogram:COMPosite {ON | OFF | 1 | 0}
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
Query Syntax
:MEASure:PJITterN:HISTogram:COMPosite?
Query Response
{1 | 0}
Description
Enables or disables the Composite PAM jitter histogram.