:MEASure:PJITter:HISTogram:DMAXimized
Command Syntax
:MEASure:PJITterN:HISTogram:DMAXimized {ON | OFF | 1 | 0}
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
Query Syntax
:MEASure:PJITterN:HISTogram:DMAXimized?
Query Response
{1 | 0}
Description
When PAM Jitter graphs are displayed in a grid (see :MEASure:PJITter:HISTogram:GSIZe), this command lets you maximize the most recently selected histogram (see :MEASure:PJITter:HISTogram:MGRaph) to occupy the space of all the grids (ON) or return to the display of graphs in a grid (OFF).