:MEASure:PJITter:HISTogram:GSIZe

Command Syntax

:MEASure:PJITterN:HISTogram:GSIZe {SMALl | MEDium | LARGe | OGRaph | OBTWo
   | TBONe | TWBTwo | TBTHree | TBTWo | THBThree}

Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.

Query Syntax

:MEASure:PJITterN:HISTogram:GSIZe?

Description

This command selects the graph size option in the PAM Jitter results content window:

  • SMALl — Auto fit small
  • MEDium — Auto fit medium
  • LARGe — Auto fit large
  • OGRaph — One graph
  • OBTWo — 1x2
  • TBONe — 2x1
  • TWBTwo — 2x2
  • TBTHree — 2x3
  • TBTWo — 3x2
  • THBThree — 3x3