:MEASure:PJITter:HISTogram:MGRaph

Command Syntax

:MEASure:PJITterN:HISTogram:MGRaph {R01 | R02 | R03 | R12 | R13 | R23
   | F10 | F20 | F30 | F21 | F31 | F32 | COMPosite}

Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.

Query Syntax

:MEASure:PJITterN:HISTogram:MGRaph?

Description

This command selects the histogram that should be maximized in the PAM Jitter window area when using the :MEASure:PJITter:HISTogram:DMAXimized command:

  • R01 — L0 to L1 Histogram
  • R02 — L0 to L2 Histogram
  • R03 — L0 to L3 Histogram
  • R12 — L1 to L2 Histogram
  • R13 — L1 to L3 Histogram
  • R23 — L0 to L1 Histogram
  • F10 — L1 to L0 Histogram
  • F20 — L2 to L0 Histogram
  • F30 — L3 to L0 Histogram
  • F21 — L2 to L1 Histogram
  • F31 — L3 to L1 Histogram
  • F32 — L3 to L2 Histogram
  • COMPosite — Composite Histogram