:NETWorks:DFILe:CLEar

Command Syntax

:NETWorks:DFILe{1:4}:CLEar

Description

Clears all S-parameters from the selected S-parameter memory. There is no command to clear all S-parameter memories. Instead, issue this command once for each of the four memories.