:NETWorks:DFILe:FILE:NAME

Command Syntax

:NETWorks:DFILeN:FILE:NAME "filename"

Where N identifies one of four {1:4} memories. For example, :NETWorks:DFILe2.

Query Syntax

:NETWorks:DFILe:FILE:NAME?

Query Response

"filename"

Description

Specifies the file (name, path, and extension) for recalling S-parameters into S-parameter memory. The default source folder is %USER_DATA_DIR%\S-Parameter Data. Use the :NETWorks:DFILe:FILE:LOAD command to actually load the file into memory. Use the query to determine the default S-parameter filename which is suggested based on the number of DUT ports.

Import File Types
File Type Description
.ts2 Touchstone 2 file. Single-ended and differential data
.s1p Touchstone 1 file. One-port single-ended device data (S11 or S22)
.s2p Touchstone 1 file. Two-port single-ended device data (S11, S21, S22, S12)
.s4p Touchstone 1 file. Four-port single-ended device data
.s8p Touchstone 1 file. Eight-port single-ended device data
.s12p Touchstone 1 file. Twelve-port single-ended device data
.s16p Touchstone 1 file. Sixteen-port single-ended device data
.txt Identical to the .s1p file type except for the .txt filename extension.