:NETWorks:DFILe:DSTatus?
Query Syntax
:NETWorks:DFILe{1:4}:DSTatus?
Query Response
{CORR | INV}
Description
Returns the status of the specified S-parameter waveform memory. Up to four memories are available. To query the reason for the current state of the memory, use the :NETWorks:DFILe:DSTatus:REASon? query. The following responses can be returned:
CORR- The S-parameter memory location contains S-parameter data. To clear memory, use the
:NETWorks:DFILe:CLEarcommand. INV- The S-parameter memory location does not contain data.