:NETWorks:DFILe:FILE:LOAD
Command Syntax
:NETWorks:DFILeN:FILE:LOAD
Where N identifies one of four {1:4} memories. For example, :NETWorks:DFILe2.
Description
Loads an S-parameter file into the destination S-parameter memory. Use the :NETWorks:DFILe:FILE:NAME command to specify the name of the S-parameter file to load. All S-parameters contained in the file will be loaded into the S-parameter memory. The default folder for S-parameter files is %USER_DATA_DIR%\S-Parameter Data.
When importing S-parameters from a file, the frequency spacing in the file must be uniform or the file will not be loaded into memory.