:NETWorks:DFILe:DSTatus:REASon?

Query Syntax

:NETWorks:DFILe{1:4}:DSTatus:REASon?

Query Response

<string>

Description

Returns a description of the status of the specified S-parameter memory. If S-parameter data are currently in the specified S-parameter memory location, the name of the source waveform will be returned. For example, "Source: Channel 1_1". If the S-parameter memory is empty, the string "Please select a file." is returned. If the file is corrupt or an incorrect type, the string "Unable to load file." is returned. To check the status of the S-parameter memory, use the :NETWorks:DFILe:DSTatus? parent query.