:NETWorks:DFILe:DSTatus:DETails?

Query Syntax

:NETWorks:DFILe{1:4}:DSTatus:DETails?

Query Response

<string>

Description

If the status of the S-parameter memory is questionable or invalid (see :NETWorks:DFILe:DSTatus?), this query returns a string that may provide additional details.

If the status of the S-parameter memory is valid, this query returns an empty string.

For a basic reason for the questionable or invalid status, use the :NETWorks:DFILe:DSTatus:REASon? sibling query.