Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:PNOise:MARKer:MARKer:MAGNitude?

:PNOise Commands
  • :PNOise Subsystem
  • :PNOise:ANNotations
  • :PNOise:CLOCk:EDGE
  • :PNOise:CORRelations
  • :PNOise:DATA:ASCii:XDATa?
  • :PNOise:DATA:ASCii:YDATa?
  • :PNOise:DATA:AVERages?
  • :PNOise:DATA:CFRequency?
  • :PNOise:DATA:CORRelations?
  • :PNOise:DATA:DOUBle:XDATa?
  • :PNOise:DATA:DOUBle:YDATa?
  • :PNOise:DATA:FLOat:XDATa?
  • :PNOise:DATA:FLOat:YDATa?
  • :PNOise:DATA:POINts?
  • :PNOise:DATA:STATus?
  • :PNOise:DATA:STYPe?
  • :PNOise:DISPlay
  • :PNOise:MARKer:LIMit
  • :PNOise:MARKer:MARKer:MAGNitude?
  • :PNOise:MARKer:MARKer:XPOSition
  • :PNOise:MARKer:STATe
  • :PNOise:PJITter?
  • :PNOise:PJITter:STARt
  • :PNOise:PJITter:STATe
  • :PNOise:PJITter:STOP
  • :PNOise:PJITter:UNITs
  • :PNOise:RSSClock
  • :PNOise:SOURce:ONE
  • :PNOise:SOURce:TWO
  • :PNOise:SOURce:TWO:ENABled
  • :PNOise:SPUR:PROCessing
  • :PNOise:SPUR:SENSitivity
  • :PNOise:WINDow
  • :PNOise:X:STARt
  • :PNOise:X:STOP
  • :PNOise:Y:OFFSet
  • :PNOise:Y:SCALe

Query Syntax

:PNOise:MARKer:MARKerN:MAGNitude?

Where N identifies one of 16 possible phase noise markers{1:16}. For example, MARKer2.

Description

When decade markers are turned on (see :PNOise:MARKer:STATe), this query will return the magnitude in dBc/Hz of the phase noise plot at a marker location (see :PNOise:MARKer:MARKer:XPOSition).