:PNOise:SOURce:ONE

Command Syntax

:PNOise:SOURce:ONE <source_waveform>

Where <source_waveform> can be one of the following:

  • CHANnel<connection1-8>_<ch1-8>; With connection 1, the "1_" part is optional, and you can simply use CHANnel<ch1-8>.
  • DIFF{1:4}
  • FUNCtion{1:64}
  • WMEMory{1:8}

Query Syntax

:PNOise:SOURce:ONE?

Description

This command selects the first signal source for the Phase Noise analysis.

Select an analog input channel (or Magnify or Average math function).

Use the :PNOise:SOURce:TWO command to select a second signal source for the Phase Noise analysis.