:PNOise:SPUR:PROCessing
Command Syntax
:PNOise:SPUR:PROCessing {NORMalized | OMIT | POWer}
Query Syntax
:PNOise:SPUR:PROCessing?
Description
This command specifies the Phase Noise analysis spurs processing option:.
NORMalized— The displayed phase noise trace treats the spurs like noise in dBc/Hz.OMIT— The displayed phase noise trace identifies and removes spurs.POWer— The displayed phase noise trace identifies and rescales spurs in dBc.
Note that the spur processing selection can affect phase jitter measurement results. See :PNOise:PJITter?.