:PNOise:MARKer:MARKer:XPOSition
Command Syntax
:PNOise:MARKer:MARKerN:XPOSition <frequency>
Where N identifies one of 16 possible phase noise markers{1:16}. For example, MARKer2.
<frequency> is a double.
Query Syntax
:PNOise:MARKer:MARKerN:XPOSition?
Description
After decade markers are turned on (see :PNOise:MARKer:STATe), this command can move a marker to non-decade boundary location.
The magnitude of the phase noise plot at a marker location can be returned by the :PNOise:MARKer:MARKer:MAGNitude? query.