:PNOise:MARKer:STATe

Command Syntax

:PNOise:MARKer:STATe {ON | OFF | 1 | 0}

Query Syntax

:PNOise:MARKer:STATe?

Query Response

{1 | 0}

Description

Turns on or off the Enable Markers Every Decade option.

When turned on, markers are automatically placed along the horizontal axis at decade boundary locations. The :PNOise:MARKer:LIMit specifies the maximum number of markers that can be placed.

The markers can be moved to non-decade boundary locations (see :PNOise:MARKer:MARKer:XPOSition).

The magnitude of the phase noise plot at a marker location can be returned by the :PNOise:MARKer:MARKer:MAGNitude? query.

To reset markers to the decade boundary positions, you can turn off and then turn back on the Enable Markers Every Decade option.