:TRIGger:AUX:SEQuence:RESet:STATe
Command Syntax
:TRIGger:AUX:SEQuence:RESet:STATe {DONTcare}
Query Syntax
:TRIGger:AUX:SEQuence:RESet:STATe?
Description
This command is reserved for when sequence trigger supports resetting by Aux Trig In input events. Currently, the only state allowed is DONTcare which means no Aux Trig In input events will reset the sequence trigger.