:TRIGger:CHANnel:SEQuence:RESet:STATe
Command Syntax
:TRIGger:CHANnelN:SEQuence:RESet:STATe {DONTcare}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:TRIGger:CHANnelN:SEQuence:RESet:STATe?
Description
This command is reserved for when sequence trigger supports resetting by channel events. Currently, the only state allowed is DONTcare which means no channel events will reset the sequence trigger.