:TRIGger:CALibrator:SEQuence:RESet:STATe
Command Syntax
:TRIGger:CALibrator:SEQuence:RESet:STATe {DONTcare}
Query Syntax
:TRIGger:CALibrator:SEQuence:RESet:STATe?
Description
This command is reserved for when sequence trigger supports resetting by calibrator output events. Currently, the only state allowed is DONTcare which means no calibrator events will reset the sequence trigger.