:TRIGger:SEQuence:RESet:LOGic

Command Syntax

:TRIGger:SEQuence:RESet:LOGic  {AND | OR}

Query Syntax

:TRIGger:SEQuence:RESet:LOGic?

Description

This command is reserved for when sequence trigger supports resetting by events. Currently, all supported events can only be set to DONTcare which means no events will reset the sequence trigger.