:TRIGger:SEQuence:RESet:TIME

Command Syntax

:TRIGger:SEQuence:RESet:TIME <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:SEQuence:RESet:TIME?

Description

When you have enabled resetting the sequence trigger by time (see :TRIGger:SEQuence:RESet:TYPE), this command specifies the amount of time to wait, after any delay time (see :TRIGger:SEQuence:DELay:TIME), before resetting the sequence.