:TRIGger:SEQuence:STATe

Command Syntax

:TRIGger:SEQuence:STATe  {OFF | ATOB}

Query Syntax

:TRIGger:SEQuence:STATe?

Description

This command selects the logic level or edge that should be included in the pattern:

  • OFF — Turns off sequence triggers.

  • ATOB — Turns on sequence triggers

    Sequence triggers let you trigger on an event that follows another event.

    The first event is called the Sequence A event. The second event is called the Sequence B event.

    You can optionally reset the trigger sequence after the Sequence A event occurs, but before the Sequence B event occurs, if a certain amount of time passes (see :TRIGger:SEQuence:RESet:TYPE).

    You can also optionally specify a delay time after the Sequence A event occurs before searching for the Sequence B event (see :TRIGger:SEQuence:DELay:TIME).