:TRIGger Edge Then Edge Commands
The Edge Then Edge trigger mode triggers on an edge event after an arming event and a delay that can be:
- A specified time. This gives you a two-edge trigger where the arming and triggering edges are separated by time.
- A specified number of occurrences of a third edge event. This gives you a multiple edge trigger where between the arming edge and the triggering edge are a number of occurrences of a third edge.