:TRIGger:DELay:MODE

Command Syntax

:TRIGger:DELay:MODE  {TIME | EVENt}

Query Syntax

:TRIGger:DELay:MODE?

Description

In the Edge Then Edge trigger mode (see :TRIGger:MODE), this command specifies whether the delay between the arm event and the trigger event is specified by time or by a number of occurrences of a third edge event.