:TRIGger:DELay:TDELay:TIME
Command Syntax
:TRIGger:DELay:TDELay:TIME <seconds>
<seconds> is a double.
Query Syntax
:TRIGger:DELay:TDELay:TIME?
Description
In the Edge Then Edge trigger mode (see :TRIGger:MODE), when Delaying By Time (see :TRIGger:DELay:MODE), this command specifies the amount of time that will qualify the delay.