:TRIGger:DELay:EDELay:SLOPe

Command Syntax

:TRIGger:DELay:EDELay:SLOPe  {POSitive | NEGative}

Query Syntax

:TRIGger:DELay:EDELay:SLOPe?

Description

In the Edge Then Edge trigger mode (see :TRIGger:MODE), when Delaying By Event (see :TRIGger:DELay:MODE), this command specifies the edge of the Delay By Event source (see :TRIGger:DELay:EDELay:SOURce) that will identify the event.