:TRIGger:DELay:TRIGger:COUNt
Command Syntax
:TRIGger:DELay:TRIGger:COUNt <occurrences>
<occurrences> is an int.
Query Syntax
:TRIGger:DELay:TRIGger:COUNt?
Description
In the Edge Then Edge trigger mode (see :TRIGger:MODE), this command specifies the Nth occurrence of the trigger source edge that will trigger.