:TRIGger:DELay:EDELay:COUNt

Command Syntax

:TRIGger:DELay:EDELay:COUNt  <occurrences>

<occurrences> is an int.

Query Syntax

:TRIGger:DELay:EDELay:COUNt?

Description

In the Edge Then Edge trigger mode (see :TRIGger:MODE), when Delaying By Event (see :TRIGger:DELay:MODE), this command specifies the number of occurrences of the specified edge event that will qualify the delay.