:TRIGger:DELay:TRIGger:SLOPe

Command Syntax

:TRIGger:DELay:TRIGger:SLOPe  {RISing | FALLing}

Query Syntax

:TRIGger:DELay:TRIGger:SLOPe?

Description

In the Edge Then Edge trigger mode (see :TRIGger:MODE), this command specifies the edge of the Trigger Source (see :TRIGger:DELay:TRIGger:SOURce) that will trigger.