:WAVeform:CGRade:ASCii:DATA?

Query Syntax

:WAVeform:CGRade:ASCii:DATA?

Query Response

The data is returned as comma-separated values.

Description

Returns color grade/gray scale database values in ASCII format. Color grade/gray scale data is transferred as a two dimensional array consisting of 521 rows by 751 columns for a total number of 391,271 points. This array corresponds to the graticule display, where each point contains a sample hit count. The array is transferred column by column, starting with the lower left corner of the graticule.

The time for any column of data points can be calculated as:

where,

The voltage for any data point at a given row (that contains a hit count) is determined by using the following equation:

where,

To transfer the data in integer values, use the :WAVeform:CGRade:INTeger:DATA? query.