:WAVeform:CGRade:UICount?
Query Syntax
:WAVeform:CGRade:UICount?
Description
Returns a string that is the number of acquired UI (unit intervals) represented in the real-time eye or color grade memory of a real-time eye identified by the :WAVeform:SOURce command.
This is the same UI count that can be seen in the graphical user interface's waveform legend.
The UI (unit interval) count can be from one or more waveforms. To get the total waveforms count represented in the real-time eye (or color grade/gray scale waveform or color grade memory), use the :WAVeform:CGRade:WCOunt? query.