:WAVeform:CGRade:WCOunt?
Query Syntax
:WAVeform:CGRade:WCOunt?
Description
Returns the number of acquired waveforms represented in the real-time eye, color grade/gray scale waveform, or color grade memory identified by the :WAVeform:SOURce command.
This is the same waveforms count that can be seen in the graphical user interface's waveform legend.
For real-time eyes, each waveform can have multiple UIs (unit intervals). To get the total UI count represented in a real-time eye or color grade memory of a real-time eye, use the :WAVeform:CGRade:UICount? query.