:WAVeform:CGRade:STATus:REASon?
Query Syntax
:WAVeform:CGRade:STATus:REASon?
Description
Queries a string that explains why the :WAVeform:CGRade:STATus? parent command indicates invalid or questionable waveform data. The following strings may be returned by this query:
- ""
- A null string indicates that the data is correct.
- "Clipped Hi"
- The amplitude of the waveform is too large and the data is clipped off the top of the screen.
- "Clipped Low"
- The amplitude of the waveform is too large and the data is clipped off the bottom of the screen.