:WAVeform:CGRade:STATus?

Query Syntax

:WAVeform:CGRade:STATus?

Description

Queries the status of the color-grade gray-scale waveform data and returns the strings shown in the following table. Use the :WAVeform:CGRade:STATus:REASon? child query to return a string that indicates why the data is invalid or questionable.

STATus? Query Response
Response Description
CORR The waveform data is correct.
INV The waveform data is invalid. Check to see if eye diagram data is displayed on the screen.
QUES The waveform data is questionable. Confirm that the eye diagram data is not clipped high, clipped low, or has holes.

Query the data using one of the following two commands:

Child Commands