:SYSTem:FACTory

Command Syntax

:SYSTem:FACTory

Description

Sets Infiniium to its factory default settings. Factory Default resets all settings including general, trigger, probe, channel skew, preferences, and instrument connection settings.

(A Default Setup resets only general and trigger settings. See :SYSTem:DEFault.)

User preference and instrument connection settings are listed in the following tables.

Use an *OPC (Operation Complete) query to pause program execution while waiting for this operation to complete.

There is no query form of this command or ability to undo its action.

Preference Settings, Miscellaneous
Feature Setting
Multi-Purpose button Removes any configuration settings

Preference Settings, Display Setup Dialog Box (Appearance Tab)
  Setting
UI Theme Tungsten
Dialog Size Normal
Overlap Display Tabs off
Use On-Screen Keyboard off

Instrument Connection Settings
Feature Setting
Connection 1 Virtual Real-Time Scope
Channel 1 Simulation Source On
Data Source: NRZ, PRBS-7, 9.95328 Gbd, 500 mV amplitude, 0 V offset
Filter: 4th order Bessel, 15 GHz bandwidth
Jitter & Noise: 100 fs random jitter, 2 mV random noise
Acquisition Run Mode On