:SYSTem:DEFault
Command Syntax
:SYSTem:DEFault
Description
Places Infiniium in a known start-up state, resetting general and trigger settings, without changing probe, channel skew, preferences, and instrument connection settings. This is the same action as using the *RST (Reset) command or clicking Infiniium's Setup > Default Setup menu command.
An autoscale is not performed.
It is a good practice to set Infiniium to its default state at the start of each program.
Use an *OPC (Operation Complete) query to pause program execution while waiting for this operation to complete.
Python Example
import pyvisa # PyVISA package
rm = pyvisa.ResourceManager()
Infiniium = rm.open_resource('TCPIP0::localhost::hislip0,4880::INSTR')
Infiniium.query(':SYSTem:DEFault;*OPC?')
Infiniium.write(':SYSTem:GTLocal')
Infiniium.close()